Debug U-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug U-boot

2,060 Views
canvanquyen
Contributor III

Hi everybody,

Currently, I'm working in B4860QDS development board.

I try to debug u-boot in this board but I have some problem bellow.

I read doc(AN4876.pdf) It guides to debug u-boot. I shows we need B4860QDS_uboot_32.tcl initialization file for B4860 chipset.

But in "C:\Freescale\CW_PA_v10.5.0\PA\PA_Support\Initialization_Files\Qonverge" directory does not have this file.

Can you tell me how i can get this file to debug u-boot on this chipset?

Thanks & best regards,

Quyen.

Labels (1)
0 Kudos
Reply
1 Reply

1,890 Views
addiyi
NXP Employee
NXP Employee

Hi Quyen,

After attach to u-boot, when uboot.tcl file is not available, you can reset the board from reset button with no initialization file.

Adrian

0 Kudos
Reply