Processor Expert report Error "Property DDR_DATA is set to a custom value"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert report Error "Property DDR_DATA is set to a custom value"

Jump to solution
1,748 Views
benoitmasse
Contributor III

Hi,

I got this error and the only info that I have is 

Description Resource Path Location Type
Property DDR_RATE is set to a custom value. LS2088ARDB-Ben1 PBL1 Problem

It is not very usefull.

I pass every section in Properties page but I did not find any custom value.

Screenshot from 2021-01-14 23-27-14.png

I attached the PBL binary file. Note I add .c to be able to upload it but it's a binary file.

Thanks

0 Kudos
Reply
1 Solution
1,735 Views
yipingwang
NXP TechSupport
NXP TechSupport

1.From Component Inspector view, select Enable/disable error checking menu, and then choose Skip error checking option, as shown in the figure below. 

 

yipingwang_0-1610952732298.png

 

 

 

 

View solution in original post

0 Kudos
Reply
1 Reply
1,736 Views
yipingwang
NXP TechSupport
NXP TechSupport

1.From Component Inspector view, select Enable/disable error checking menu, and then choose Skip error checking option, as shown in the figure below. 

 

yipingwang_0-1610952732298.png

 

 

 

 

0 Kudos
Reply