Processor Expert report Error "Property DDR_DATA is set to a custom value"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert report Error "Property DDR_DATA is set to a custom value"

ソリューションへジャンプ
1,741件の閲覧回数
benoitmasse
Contributor III

Hi,

I got this error and the only info that I have is 

Description Resource Path Location Type
Property DDR_RATE is set to a custom value. LS2088ARDB-Ben1 PBL1 Problem

It is not very usefull.

I pass every section in Properties page but I did not find any custom value.

Screenshot from 2021-01-14 23-27-14.pngScreenshot from 2021-01-14 23-27-14.png

I attached the PBL binary file. Note I add .c to be able to upload it but it's a binary file.

Thanks

0 件の賞賛
返信
1 解決策
1,728件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

1.From Component Inspector view, select Enable/disable error checking menu, and then choose Skip error checking option, as shown in the figure below. 

 

yipingwang_0-1610952732298.pngyipingwang_0-1610952732298.png

 

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,729件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

1.From Component Inspector view, select Enable/disable error checking menu, and then choose Skip error checking option, as shown in the figure below. 

 

yipingwang_0-1610952732298.pngyipingwang_0-1610952732298.png

 

 

 

 

0 件の賞賛
返信