Processor Expert fails to generate code with MQX as RTOS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Processor Expert fails to generate code with MQX as RTOS

跳至解决方案
4,148 次查看
CraigCo
Contributor III

"Generator: FAILURE: Unexpected status of script: Drivers\Common\PE_MisraEnableRules.prg, please contact Freescale support."

I'm attempting to clone the BSP from twrk20d50m. The end result would be to move to an MK10DN32VLF5. I'm following the IAR section of "MQX_BSP_Porting_Example_User_Guide" from the MQX 4.1 release. The error above occurs at step 4.1.3. Just to clarify, this happens before I change anything after re-using the CodeWarrior project settings (besides changing the compiler to IAR).

What I have tried:

Using MQX 4.0 and 4.1

Deleting the port and restarting ensuring every step was followed correctly

Replacing the OS with MQX-Lite : It successfully generates code.

Closing and Opening the project

Restarting PEx

Uninstalling and Reinstalling PEx.

Porting from twrk60n512: I can generate the code with MQX as the RTOS without the error

Attempting to locate the "PE_MisraEnableRules.prg", cannot find it. (perhaps my problem)


OS: Windows 7 Professional (32-bit)


0 项奖励
回复
1 解答
3,936 次查看
Petr_H
NXP Employee
NXP Employee

Hi,

this is most probably a known issue. Please see the thread PE 10.4 Error in PE_MisraEnableRules.prg where the hotfix for DS 10.4  has been published.

Best regards

Petr Hradsky

Processor Expert Support Team

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,936 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Craig,

what's PE software do you working with? can you try the latest 10.4?

Microcontrollers Driver Suite v10.4

how does this version work?

==========================================================

this answer is for you. if it helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

0 项奖励
回复
3,936 次查看
CraigCo
Contributor III

Thanks for your response and for asking about the version of PEx as I forgot to mention it. I am in fact using 10.4, unfortunately. Too bad it's not that easy. Thanks for the thought though.

0 项奖励
回复
3,937 次查看
Petr_H
NXP Employee
NXP Employee

Hi,

this is most probably a known issue. Please see the thread PE 10.4 Error in PE_MisraEnableRules.prg where the hotfix for DS 10.4  has been published.

Best regards

Petr Hradsky

Processor Expert Support Team

0 项奖励
回复
3,936 次查看
CraigCo
Contributor III

Petr_H

You are absolutely correct! Apparently my googling skills need work as I had not found that thread. I applied the hotfix and the problem is solved.

Thanks!

0 项奖励
回复