Processor Expert fails to generate code with MQX as RTOS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert fails to generate code with MQX as RTOS

Jump to solution
4,117 Views
CraigCo
Contributor III

"Generator: FAILURE: Unexpected status of script: Drivers\Common\PE_MisraEnableRules.prg, please contact Freescale support."

I'm attempting to clone the BSP from twrk20d50m. The end result would be to move to an MK10DN32VLF5. I'm following the IAR section of "MQX_BSP_Porting_Example_User_Guide" from the MQX 4.1 release. The error above occurs at step 4.1.3. Just to clarify, this happens before I change anything after re-using the CodeWarrior project settings (besides changing the compiler to IAR).

What I have tried:

Using MQX 4.0 and 4.1

Deleting the port and restarting ensuring every step was followed correctly

Replacing the OS with MQX-Lite : It successfully generates code.

Closing and Opening the project

Restarting PEx

Uninstalling and Reinstalling PEx.

Porting from twrk60n512: I can generate the code with MQX as the RTOS without the error

Attempting to locate the "PE_MisraEnableRules.prg", cannot find it. (perhaps my problem)


OS: Windows 7 Professional (32-bit)


0 Kudos
Reply
1 Solution
3,905 Views
Petr_H
NXP Employee
NXP Employee

Hi,

this is most probably a known issue. Please see the thread PE 10.4 Error in PE_MisraEnableRules.prg where the hotfix for DS 10.4  has been published.

Best regards

Petr Hradsky

Processor Expert Support Team

View solution in original post

0 Kudos
Reply
4 Replies
3,905 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Craig,

what's PE software do you working with? can you try the latest 10.4?

Microcontrollers Driver Suite v10.4

how does this version work?

==========================================================

this answer is for you. if it helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

0 Kudos
Reply
3,905 Views
CraigCo
Contributor III

Thanks for your response and for asking about the version of PEx as I forgot to mention it. I am in fact using 10.4, unfortunately. Too bad it's not that easy. Thanks for the thought though.

0 Kudos
Reply
3,906 Views
Petr_H
NXP Employee
NXP Employee

Hi,

this is most probably a known issue. Please see the thread PE 10.4 Error in PE_MisraEnableRules.prg where the hotfix for DS 10.4  has been published.

Best regards

Petr Hradsky

Processor Expert Support Team

0 Kudos
Reply
3,905 Views
CraigCo
Contributor III

Petr_H

You are absolutely correct! Apparently my googling skills need work as I had not found that thread. I applied the hotfix and the problem is solved.

Thanks!

0 Kudos
Reply