How to assign data bus and address bus on diffrent pins like non multiplexing mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to assign data bus and address bus on diffrent pins like non multiplexing mode

Jump to solution
2,550 Views
MK60FX512
Contributor I

How to assign data bus and address bus on diffrent pins like non multiplexing mode in Processor expert for K60 MCU?

0 Kudos
Reply
1 Solution
1,837 Views
Petr_H
NXP Employee
NXP Employee

It's a limitation of Processor Expert that only shared bus can be used. We are planning to improve this in the future versions.

You can find a way of configuring the bus without using Processor Expert in the following application note : http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4393.pdf

best regards

Petr Hradsky

Processor Expert Support Team

View solution in original post

0 Kudos
Reply
3 Replies
1,838 Views
Petr_H
NXP Employee
NXP Employee

It's a limitation of Processor Expert that only shared bus can be used. We are planning to improve this in the future versions.

You can find a way of configuring the bus without using Processor Expert in the following application note : http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4393.pdf

best regards

Petr Hradsky

Processor Expert Support Team

0 Kudos
Reply
1,837 Views
adamcrha
Contributor I

Hello Petr,

any improovement in this feature? It is almost 3 years you said you are planning to improve this in the future versions. I have "Processor Expert for Kinetis    3.0.0.RT7_b1515-0427" and can't still set non-multiplexed flexbus.

Thank you

0 Kudos
Reply
1,837 Views
MK60FX512
Contributor I

Thanks for infomation

but it is take lot time to understand/read the application note or datasheet.

It should be implemented in some GUI like Processor expert. all other company is giving same way like infineon DAVE tool.

0 Kudos
Reply