How to assign data bus and address bus on diffrent pins like non multiplexing mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to assign data bus and address bus on diffrent pins like non multiplexing mode

ソリューションへジャンプ
2,566件の閲覧回数
MK60FX512
Contributor I

How to assign data bus and address bus on diffrent pins like non multiplexing mode in Processor expert for K60 MCU?

0 件の賞賛
返信
1 解決策
1,853件の閲覧回数
Petr_H
NXP Employee
NXP Employee

It's a limitation of Processor Expert that only shared bus can be used. We are planning to improve this in the future versions.

You can find a way of configuring the bus without using Processor Expert in the following application note : http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4393.pdf

best regards

Petr Hradsky

Processor Expert Support Team

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,854件の閲覧回数
Petr_H
NXP Employee
NXP Employee

It's a limitation of Processor Expert that only shared bus can be used. We are planning to improve this in the future versions.

You can find a way of configuring the bus without using Processor Expert in the following application note : http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4393.pdf

best regards

Petr Hradsky

Processor Expert Support Team

0 件の賞賛
返信
1,853件の閲覧回数
adamcrha
Contributor I

Hello Petr,

any improovement in this feature? It is almost 3 years you said you are planning to improve this in the future versions. I have "Processor Expert for Kinetis    3.0.0.RT7_b1515-0427" and can't still set non-multiplexed flexbus.

Thank you

0 件の賞賛
返信
1,853件の閲覧回数
MK60FX512
Contributor I

Thanks for infomation

but it is take lot time to understand/read the application note or datasheet.

It should be implemented in some GUI like Processor expert. all other company is giving same way like infineon DAVE tool.

0 件の賞賛
返信