Error when disable interrupt of ADC component (Processor Expert)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Error when disable interrupt of ADC component (Processor Expert)

跳至解决方案
2,150 次查看
henryxin
Contributor II

Hi,

I am doing some test with KLZ25 board with Processor Export.

When I add a ADC component, it works well.

enable.png

but when I disable its interrupt, there will be an error:

disable.png

I can not figure out the problem. Does it mean I can not disable the ADC interrupt?

Thanks,

Henry Xin

0 项奖励
回复
1 解答
1,981 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi henry,

Please update the Processor Expert Software : help -> Install New Software,

pastedImage_0.png

and i recommend you updated other related software if you use .

On my side , there is no error refer to you said to configure :

pastedImage_1.png

Best Regards,

Alice

------------------------------------------------------------------------------------------

If this post answers your question, please click the Correct Answer button.

-----------------------------------------------------------------------------------

If this post help your question, please click the helpful Answer button.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
1,981 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Henry,

On my side , when only add the ADC_LDD component , disable the interrupt , there is no error :

pastedImage_0.png

Please tell me which Processor Expert you use ?

And i think it is maybe not the problem of disable the interrupt.

Please create a simple project ,only add the ADC component, then test it .If still have error , please send you project to me , i will test it on my side .


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,981 次查看
henryxin
Contributor II

Hi Alice,

Thanks for your reply.

But I tried to create a simple project which only has an ADC component, and still got error as:
adc_error.png

Following is my PE version information:

Processor Expert Software,

Microcontroller Driver Suite

(c) Copyright Freescale Semiconductor, Inc. All rights reserved.

http://www.freescale.com/processorexpert

Version: 10.4.0

Build: b140319

BR

Henry

0 项奖励
回复
1,981 次查看
henryxin
Contributor II

By the way I used the ADC component in the "CPU Internal Peripherals" category, not in the "Logical Device drivers" category.

Thanks,
Henry

0 项奖励
回复
1,982 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi henry,

Please update the Processor Expert Software : help -> Install New Software,

pastedImage_0.png

and i recommend you updated other related software if you use .

On my side , there is no error refer to you said to configure :

pastedImage_1.png

Best Regards,

Alice

------------------------------------------------------------------------------------------

If this post answers your question, please click the Correct Answer button.

-----------------------------------------------------------------------------------

If this post help your question, please click the helpful Answer button.

0 项奖励
回复
1,981 次查看
henryxin
Contributor II

Hi Alice,

After updating the PE, It works well with me.

Thank you very much.

Henry

0 项奖励
回复