DMA maximum transfer count using nested transfers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DMA maximum transfer count using nested transfers

Jump to solution
3,515 Views
mattyd
Contributor I

Hi,

 

I am using the PK60N512VMD100 tower with processor expert.

 

I have created a module that uses the DMA to transfer n 16-bit ADC samples to memory. I have set value in data size of the DMATransfer_LDD (which seems to be for the minor loop register) to 2 and transfer count of transfer control to be n. When I choose a value greater than 256, the memory buffers are not filled by the DMA beyond the 256th entry in memory.

 

It seems that the CITER register related to the major loop register is only 8-bits wide. However, documentation states that it can be as many as 14-bits wide if channel linking is not used on the DMA. Is there an explanation for this? Or am I misreading the K60 manual.

 

Thanks,

Matty D

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,196 Views
ProcessorExpert
Senior Contributor III

Hello,

 

we are aware of this problem, the fix would be published soon within CW V10.2 update.

 

In mean-time you can use the hot-fix that I have sent you direcly by email. The forum does not allow me to upload large files.

 

best regards
Vojtech Filip
Processor Expert Support Team

View solution in original post

0 Kudos
Reply
3 Replies
3,197 Views
ProcessorExpert
Senior Contributor III

Hello,

 

we are aware of this problem, the fix would be published soon within CW V10.2 update.

 

In mean-time you can use the hot-fix that I have sent you direcly by email. The forum does not allow me to upload large files.

 

best regards
Vojtech Filip
Processor Expert Support Team

0 Kudos
Reply
3,196 Views
mattyd
Contributor I

So I gave it a try and the hot fix solved this problem.

 

Thanks!!

 

Matty D

0 Kudos
Reply
3,196 Views
mattyd
Contributor I

Thanks, I will give it a try.

 

Matthew

0 Kudos
Reply