CAN_LDD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,581件の閲覧回数
carrielbr
Contributor II

To initialize the component in function CAN1_Init(NULL);

the boot is locked on the line while ( CAN_PDD_GetSoftResetState ( CAN0_BASE_PTR ) == CAN_PDD_NOT_RESET ) {}
Do what ?

タグ(4)
0 件の賞賛
返信
1 解決策
2,150件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

Could you provide more details about your application (and also the application) for analysis, please?

For example the issue can be cause by incorrect settings of clock (using of clock source that is not configured properly or external crystal does not work).

Best Regards,

Marek Neuzil

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,151件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

Could you provide more details about your application (and also the application) for analysis, please?

For example the issue can be cause by incorrect settings of clock (using of clock source that is not configured properly or external crystal does not work).

Best Regards,

Marek Neuzil

0 件の賞賛
返信
2,150件の閲覧回数
carrielbr
Contributor II

External crystal not work.

Thanks

0 件の賞賛
返信