CAN_LDD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
2,756 Views
carrielbr
Contributor I

To initialize the component in function CAN1_Init(NULL);

the boot is locked on the line while ( CAN_PDD_GetSoftResetState ( CAN0_BASE_PTR ) == CAN_PDD_NOT_RESET ) {}
Do what ?

0 Kudos
Reply
1 Solution
2,325 Views
marek_neuzil
NXP Employee
NXP Employee

Hello,

Could you provide more details about your application (and also the application) for analysis, please?

For example the issue can be cause by incorrect settings of clock (using of clock source that is not configured properly or external crystal does not work).

Best Regards,

Marek Neuzil

View solution in original post

0 Kudos
Reply
2 Replies
2,326 Views
marek_neuzil
NXP Employee
NXP Employee

Hello,

Could you provide more details about your application (and also the application) for analysis, please?

For example the issue can be cause by incorrect settings of clock (using of clock source that is not configured properly or external crystal does not work).

Best Regards,

Marek Neuzil

0 Kudos
Reply
2,325 Views
carrielbr
Contributor I

External crystal not work.

Thanks

0 Kudos
Reply