Load some data into the Data RAM memory in MC33PT2000?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Load some data into the Data RAM memory in MC33PT2000?

ソリューションへジャンプ
2,472件の閲覧回数
Borden
Contributor III

MC33PT2000, During program execution, need to modify some data in DATARAM. While debugging, it was discovered that rewriting all 192 data  to DATARAM was the only effective method. Is it possible to change a specific data in DATARAM Using a simple method? How can the code be written?

DataRAMChangeData.png

ラベル(1)
0 件の賞賛
返信
1 解決策
2,430件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Hongyu,

please use the PSC simulator. Please check the videos in this link. Please also check the section 8.1.2.2 in the PT2000 datasheet.

JozefKozon_0-1725346627507.png

 

With Best Regards,

Jozef

元の投稿で解決策を見る

4 返答(返信)
2,453件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Hongyu,

the DataRAM access is described in the section 2.8 in the PT2000SWUG attached. Please refer to it.

With Best Regards,

Jozef

0 件の賞賛
返信
2,436件の閲覧回数
Borden
Contributor III
Thank you! But, I didn't describe it clearly. Actually, I want to enable real-time data exchange between the microcontroller (for example: S32K144) and the MC33PT2000 (writing data to DATARAM). What method should I use?
0 件の賞賛
返信
2,431件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Hongyu,

please use the PSC simulator. Please check the videos in this link. Please also check the section 8.1.2.2 in the PT2000 datasheet.

JozefKozon_0-1725346627507.png

 

With Best Regards,

Jozef

2,421件の閲覧回数
Borden
Contributor III
Thanks!
0 件の賞賛
返信