Load some data into the Data RAM memory in MC33PT2000?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Load some data into the Data RAM memory in MC33PT2000?

跳至解决方案
2,481 次查看
Borden
Contributor III

MC33PT2000, During program execution, need to modify some data in DATARAM. While debugging, it was discovered that rewriting all 192 data  to DATARAM was the only effective method. Is it possible to change a specific data in DATARAM Using a simple method? How can the code be written?

DataRAMChangeData.png

标签 (1)
0 项奖励
回复
1 解答
2,439 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Hongyu,

please use the PSC simulator. Please check the videos in this link. Please also check the section 8.1.2.2 in the PT2000 datasheet.

JozefKozon_0-1725346627507.png

 

With Best Regards,

Jozef

在原帖中查看解决方案

4 回复数
2,462 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Hongyu,

the DataRAM access is described in the section 2.8 in the PT2000SWUG attached. Please refer to it.

With Best Regards,

Jozef

0 项奖励
回复
2,445 次查看
Borden
Contributor III
Thank you! But, I didn't describe it clearly. Actually, I want to enable real-time data exchange between the microcontroller (for example: S32K144) and the MC33PT2000 (writing data to DATARAM). What method should I use?
0 项奖励
回复
2,440 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Hongyu,

please use the PSC simulator. Please check the videos in this link. Please also check the section 8.1.2.2 in the PT2000 datasheet.

JozefKozon_0-1725346627507.png

 

With Best Regards,

Jozef

2,430 次查看
Borden
Contributor III
Thanks!
0 项奖励
回复