Hi Yiping Wang,
Thank you for taking the time to answer. I had tried doing what you suggest above but oprofile seems to be dependent on popt, which I cannot control.
The Package list shows --- popt
I believe this means the popt is included because of the dependency...and popt requires gettext, which I also included. Building with these package added (oprofile, popt and gettext) results in the following error:
checking mcheck.h usability... yes
checking mcheck.h presence... yes
checking for mcheck.h... yes
checking for unistd.h... (cached) yes
checking for /usr/ucblib in LIBS... no
checking for GNU xgettext... configure: error:
*** GNU gettext is required. The latest version
*** is always available from ftp://ftp.gnu.org/gnu/gettext/.
error: Bad exit status from /opt/freescale/ltib-mpc8308erdb-20100413/ltib-mpc8308erdb-zmi/tmp/rpm-tmp.99998 (%build)
RPM build errors:
Bad exit status from /opt/freescale/ltib-mpc8308erdb-20100413/ltib-mpc8308erdb-zmi/tmp/rpm-tmp.99998 (%build)
Build time for popt: 3 seconds
Failed building popt
f_buildrpms() returned an error, exiting
traceback:
main:560
Started: Mon Jun 9 15:36:28 2014
Ended: Mon Jun 9 15:37:41 2014
Elapsed: 73 seconds
These packages failed to build:
popt
Build Failed
Exiting on error or interrupt
zmi@debian:/opt/freescale/ltib-mpc8308erdb-20100413/ltib-mpc8308erdb-zmi$
Any ideas?
Thanks again,
Stacy