Why MPC8306SOM using Flash m29W640gt ,but can't find the device in CW8.8 programmer device list.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Why MPC8306SOM using Flash m29W640gt ,but can't find the device in CW8.8 programmer device list.

跳至解决方案
1,835 次查看
00lirui
Contributor I

   Why MPC8306SOM using Flash m29W640gt ,but can't find the device in CW8.8 programmer device list??

0 项奖励
回复
1 解答
1,703 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Li Rui,

It uses flash algorithm of M29W640DB, please refer to the template file in C:\Program Files\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC\83xx, and which uses "amd" flash algorithm in C:\Program Files\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC, you could find the information from C:\Program Files\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC\FPDeviceConfig.xml.

Actually in your previous thread, I didn't think it was flash algorithm problem.

Would you please provide more detailed information in the previous thread?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,704 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Li Rui,

It uses flash algorithm of M29W640DB, please refer to the template file in C:\Program Files\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC\83xx, and which uses "amd" flash algorithm in C:\Program Files\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC, you could find the information from C:\Program Files\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC\FPDeviceConfig.xml.

Actually in your previous thread, I didn't think it was flash algorithm problem.

Would you please provide more detailed information in the previous thread?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复