Why MPC8306SOM using Flash m29W640gt ,but can't find the device in CW8.8 programmer device list.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why MPC8306SOM using Flash m29W640gt ,but can't find the device in CW8.8 programmer device list.

ソリューションへジャンプ
1,869件の閲覧回数
00lirui
Contributor I

   Why MPC8306SOM using Flash m29W640gt ,but can't find the device in CW8.8 programmer device list??

0 件の賞賛
返信
1 解決策
1,737件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Li Rui,

It uses flash algorithm of M29W640DB, please refer to the template file in C:\Program Files\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC\83xx, and which uses "amd" flash algorithm in C:\Program Files\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC, you could find the information from C:\Program Files\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC\FPDeviceConfig.xml.

Actually in your previous thread, I didn't think it was flash algorithm problem.

Would you please provide more detailed information in the previous thread?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,738件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Li Rui,

It uses flash algorithm of M29W640DB, please refer to the template file in C:\Program Files\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC\83xx, and which uses "amd" flash algorithm in C:\Program Files\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC, you could find the information from C:\Program Files\Freescale\CodeWarrior PA V8.8\bin\Plugins\Support\Flash_Programmer\EPPC\FPDeviceConfig.xml.

Actually in your previous thread, I didn't think it was flash algorithm problem.

Would you please provide more detailed information in the previous thread?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信