TLB was setup correctly but the virtual address has no effect. The virtual address is still the real address.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TLB was setup correctly but the virtual address has no effect. The virtual address is still the real address.

1,058件の閲覧回数
qinghuazhou
Contributor I

In TLB the virtual address is not the same as the real addresss.@

0 件の賞賛
返信
2 返答(返信)

912件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

What do you think about specifying which processor you are using?

MMU block may differ from processor to processor.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

912件の閲覧回数
qinghuazhou
Contributor I

The processor is MPC603E. The system memory is 4MB.

0 件の賞賛
返信