TLB was setup correctly but the virtual address has no effect. The virtual address is still the real address.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TLB was setup correctly but the virtual address has no effect. The virtual address is still the real address.

1,035 Views
qinghuazhou
Contributor I

In TLB the virtual address is not the same as the real addresss.@

0 Kudos
Reply
2 Replies

889 Views
alexander_yakov
NXP Employee
NXP Employee

What do you think about specifying which processor you are using?

MMU block may differ from processor to processor.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

889 Views
qinghuazhou
Contributor I

The processor is MPC603E. The system memory is 4MB.

0 Kudos
Reply