TLB was setup correctly but the virtual address has no effect. The virtual address is still the real address.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TLB was setup correctly but the virtual address has no effect. The virtual address is still the real address.

1,066 次查看
qinghuazhou
Contributor I

In TLB the virtual address is not the same as the real addresss.@

0 项奖励
回复
2 回复数

920 次查看
alexander_yakov
NXP Employee
NXP Employee

What do you think about specifying which processor you are using?

MMU block may differ from processor to processor.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

920 次查看
qinghuazhou
Contributor I

The processor is MPC603E. The system memory is 4MB.

0 项奖励
回复