Signals of CodeWarrior USB TAP Connector.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Signals of CodeWarrior USB TAP Connector.

1,209 次查看
frankzh
Contributor I

I'm looking at my USB TAP (CWH-UTP-PPCC-HE) and is confused by the Pins of the connector. The red signal of the ribbon is the first one on the upper side. Does that denote Pin 1? I'm asking because I can't find the user manual for it. The only one I found is CodeWarrior USB TAP Probe, which has the red signal as the last one on the lower side of the ribbon.

Btw, where can I download the driver for CWH-UTP-PPCC-HE?

IMG_20151118_172615.jpg

标记 (2)
0 项奖励
回复
2 回复数

1,066 次查看
LPP
NXP Employee
NXP Employee

Red stipe denotes Pin 1 of the COP connector.

The USBTAP driver is provided with CodeWarrior and it is typically installed during CW setup.

You can remove/reinstall it following instruction at \CW PA V8.8\ccs\drivers\usb\resdme.txt


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,066 次查看
frankzh
Contributor I

Thank you Pavel.

0 项奖励
回复