Signals of CodeWarrior USB TAP Connector.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Signals of CodeWarrior USB TAP Connector.

1,308件の閲覧回数
frankzh
Contributor I

I'm looking at my USB TAP (CWH-UTP-PPCC-HE) and is confused by the Pins of the connector. The red signal of the ribbon is the first one on the upper side. Does that denote Pin 1? I'm asking because I can't find the user manual for it. The only one I found is CodeWarrior USB TAP Probe, which has the red signal as the last one on the lower side of the ribbon.

Btw, where can I download the driver for CWH-UTP-PPCC-HE?

IMG_20151118_172615.jpg

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,165件の閲覧回数
LPP
NXP Employee
NXP Employee

Red stipe denotes Pin 1 of the COP connector.

The USBTAP driver is provided with CodeWarrior and it is typically installed during CW setup.

You can remove/reinstall it following instruction at \CW PA V8.8\ccs\drivers\usb\resdme.txt


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,165件の閲覧回数
frankzh
Contributor I

Thank you Pavel.

0 件の賞賛
返信