P4080DS UART No Output

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P4080DS UART No Output

1,156 次查看
yyurtcan
Contributor III

Hi,

I have board based on p4080ds. When I power on board, there is no output from uart. I checked duart registers and I found that BI status is interrupted in the ULSR1 register and RXRDY status is not ready in the UDSR1 register.  I could not find what are the reasons for that?

Best regards.

标记 (2)
0 项奖励
回复
1 回复

1,073 次查看
alexander_yakov
NXP Employee
NXP Employee

BI means break condition - Rx line was held in logic "zero" for more than character time.

The reason, why RXRDY is cleared is specified in Table 17-106 "UDSR[RXRDY] Cleared Conditions" of P4080 Reference Manual.

P4080 Reference Manual (P4080RM) is available from P4080 product page, "Documentation" tab:

QorIQ® P4080|NXP 


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------