P4080DS UART No Output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P4080DS UART No Output

1,585件の閲覧回数
yyurtcan
Contributor III

Hi,

I have board based on p4080ds. When I power on board, there is no output from uart. I checked duart registers and I found that BI status is interrupted in the ULSR1 register and RXRDY status is not ready in the UDSR1 register.  I could not find what are the reasons for that?

Best regards.

タグ(2)
0 件の賞賛
返信
1 返信

1,502件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

BI means break condition - Rx line was held in logic "zero" for more than character time.

The reason, why RXRDY is cleared is specified in Table 17-106 "UDSR[RXRDY] Cleared Conditions" of P4080 Reference Manual.

P4080 Reference Manual (P4080RM) is available from P4080 product page, "Documentation" tab:

QorIQ® P4080|NXP 


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------