Max DDR2 clock of MPC8349 with 533 MHz CSB?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Max DDR2 clock of MPC8349 with 533 MHz CSB?

1,336件の閲覧回数
EAlepins
Contributor V

Hi,

MPC8349EA Hardware Specifications Rev 13 says in note 4 of Table 66 that "AJF marked parts support DDR1 and DDR2 data rate up to 333 MHz (at a CSB of 333 MHz)." However, Table 57 says that AJF devices (i.e. 533 MHz core freq devices), maximum DDR2 frequency is 133 MHz. Contradiction?

Thanks,

Étienne

ラベル(2)
0 件の賞賛
返信
1 返信

1,295件の閲覧回数
Bulat
NXP Employee
NXP Employee

Yes, table 57 is not correct, DDR memory bus frequency should be 100 - 166.67MHz for 533MHz devices.

Regards,

Bulat

0 件の賞賛
返信