sdram data swapping

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sdram data swapping

2,427 Views
Pamid
Contributor II

I would like to know MPC885  databus(31:0) connectivity   to SDRAM  MT48LC2M32. Shall we need to connect D0 of MPC885 to D0 of SDRAM or D0 of mpc885 to d31 of SDRAM. As mpc885 is in big-endian  mode and connecting MPC885 A29--> SDRAM A0. as far as data bus is concerned  we need clarification.

Labels (1)
0 Kudos
Reply
1 Reply

2,375 Views
r8070z
NXP Employee
NXP Employee

You can swap byte lanes and bits inside byte lane as you want. For example you can connect byte lane D0, D1, D2..D7, BS0 of the MPC885 to D15, D13, D14…D8, DQM1 of the SDRAM MT48LC2M32. The MPC885 reads the same byte what it writes.

0 Kudos
Reply