Hi,
MPC8349EA Hardware Specifications Rev 13 says in note 4 of Table 66 that "AJF marked parts support DDR1 and DDR2 data rate up to 333 MHz (at a CSB of 333 MHz)." However, Table 57 says that AJF devices (i.e. 533 MHz core freq devices), maximum DDR2 frequency is 133 MHz. Contradiction?
Thanks,
Étienne
Yes, table 57 is not correct, DDR memory bus frequency should be 100 - 166.67MHz for 533MHz devices.
Regards,
Bulat