How to test NVRAM in Yacto Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to test NVRAM in Yacto Linux

ソリューションへジャンプ
3,073件の閲覧回数
vinothkumars
Senior Contributor IV

Hi All,

I am using Power PC and I want to test NVRAM.

1> Is it any commands to test nvram in command prompt ?

2> How to write, read and erase NVRAM ?

Regards,

VinothS

Regards,
Vinothkumar Sekar
タグ(2)
0 件の賞賛
返信
1 解決策
2,688件の閲覧回数
Pavel
NXP Employee
NXP Employee

Often u-boot is used for RAM test.

U-boot contains simple memory test.

See the following pages:

https://github.com/LeMaker/u-boot/blob/master/doc/README.memory-test

 

http://www.denx.de/wiki/publish/DULG/to-delete/UBootCmdGroupMemory.html

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,689件の閲覧回数
Pavel
NXP Employee
NXP Employee

Often u-boot is used for RAM test.

U-boot contains simple memory test.

See the following pages:

https://github.com/LeMaker/u-boot/blob/master/doc/README.memory-test

 

http://www.denx.de/wiki/publish/DULG/to-delete/UBootCmdGroupMemory.html

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,688件の閲覧回数
vinothkumars
Senior Contributor IV

Thank you Pavel, I closed this thread now.

Regards,
Vinothkumar Sekar
0 件の賞賛
返信