CodeWarrior8.8 for CodeWarrior TAP,MPC8309

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior8.8 for CodeWarrior TAP,MPC8309

ソリューションへジャンプ
4,158件の閲覧回数
tom3721
Contributor I

The software I used to use was Code Warrior8.8, and the emulator I used was CodeWarrior USB TAP. Now I have purchased CodeWarrior TAP, but this emulator cannot be correctly recognized in Code Warrior 8.8. Is there any additional program to correct this?

0 件の賞賛
返信
1 解決策
4,153件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

You need to apply Patch 8.8.6 to update CodeWarrior CCS USB driver to support CodeWarrior TAP.

Please login https://www.nxp.com, then download Patch 8.8.6 from "My NXP Account->Software Licensing and Support->View accounts->NXP Software->CodeWarrior Networked Suite - Specialist Level -> 8.8 CodeWarrior DS for Power Architecture, Professional Edition (Windows Hosted) WIN->Software Patch: CW PA v8.8.6 Windows - Patch.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,780件の閲覧回数
laohu113
Contributor I

Hello, I have the same situation as you, but after I installed the patch, the result is the same as before, do you remember there are some special steps?

0 件の賞賛
返信
3,773件の閲覧回数
tom3721
Contributor I

我安装了补丁后就能正常使用了,没有碰到其它问题。

0 件の賞賛
返信
4,154件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

You need to apply Patch 8.8.6 to update CodeWarrior CCS USB driver to support CodeWarrior TAP.

Please login https://www.nxp.com, then download Patch 8.8.6 from "My NXP Account->Software Licensing and Support->View accounts->NXP Software->CodeWarrior Networked Suite - Specialist Level -> 8.8 CodeWarrior DS for Power Architecture, Professional Edition (Windows Hosted) WIN->Software Patch: CW PA v8.8.6 Windows - Patch.

0 件の賞賛
返信
4,150件の閲覧回数
tom3721
Contributor I

Thank you very much. The problem has been solved after installing the patch.

0 件の賞賛
返信