CWH-UTP-ONCE-HE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CWH-UTP-ONCE-HE

1,254件の閲覧回数
chiilokwong
Contributor I

Hi,

I have bought CodeWarrior USB TAP version CWH-UTP-ONCE-HE to flash and debugging purpose for MPC8260.

I realized that I bought wrong type of USB TAP.

Question1: Is there's someway convert my current CWH-UTP-ONCE-HE to support JTAG/COP interface by add 16pin cable inside the USB TAP?

Question2: Please guide me how to upload/read firmware to MPC8260.

Regards,

Lok

0 件の賞賛
返信
1 返信

1,124件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

1. No, there is no way to convert "ONCE" version of USBTAP to "COP" version, we do not support this.

2. The recommended way to upload firmware to MPC8260 board is to use "Flash Programmer", which is a part of our CodeWarrior IDE (software) .CodeWarrior software should be used with CodeWarrior debig probe("CodeWarrior TAP" or "CodeWarrior USB TAP"). "CodeWarrior TAP" debug probe supports different debug probe tips, in case of "CodeWarrior USB TAP" you have to order proper "COP" version of USB TAP.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信