Blocked using Trace32 u-boot debugging and problem with hardware breakpoint

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Blocked using Trace32 u-boot debugging and problem with hardware breakpoint

Jump to solution
3,579 Views
vinothkumars
Senior Contributor IV

Hi All,

We are debugging u-boot using trace32 on our new processor board with an T4240RDB.

 

We are currently blocked in our development. We are having problems with Trace32 debugger

hardware breakpoints

 

Here the situation:

    We understand that in order to get hardware breakpoints to work we need:

   1- A valid address with a valid instruction at IPVR

   2- DE bit enable in MSR register

   3- To avoid problems; always set breakpoints before or after code which accesses SRR0 and SRR1, and never step         through such code.

We have also verify that:

  • Address Space is 1 (MSR IS and DS are both set to 1),
  • Debug interrupt is enable (MSR DE is 1), and
  • The effect of the TLB update is visible (rfi instruction should cause this to occur).

u-boot,

 

        lis     r6,MSR_IS|MSR_IS|MSR_DS|MSR_IS|MSR_DE@h

        ori     r6,r6,MSR_IS|MSR_IS|MSR_DS|MSR_IS|MSR_DE@l

        lis     r7,switch_as@h

        ori     r7,r7,switch_as@l

 

        mtspr   SPRN_SRR0,r7

        mtspr   SPRN_SRR1,r6

        rfi

After rfi instruction, jump to 0xEFFFF574 but, there is no data present and also all address same like that (data :??????????????)

Thank you,

VinothS

Regards,
Vinothkumar Sekar
Labels (1)
0 Kudos
Reply
1 Solution
3,386 Views
vinothkumars
Senior Contributor IV

Hi Reinhard,

Thank for your reply and Instruction execute when change MSR to 0.

Regards, VinothS

Regards,
Vinothkumar Sekar

View solution in original post

0 Kudos
Reply
3 Replies
3,386 Views
rweiss
Contributor V

Hi VinothS,

it seems some of the prerequisites you mention are for e500 cores and do not apply to e500mc/e5500/e6500 cores.

Please contact your local TRACE32 FAE for assistance. You can find the contact information here:

TRACE32® Worldwide Representation 

Best regards,

Reinhard

0 Kudos
Reply
3,387 Views
vinothkumars
Senior Contributor IV

Hi Reinhard,

Thank for your reply and Instruction execute when change MSR to 0.

Regards, VinothS

Regards,
Vinothkumar Sekar
0 Kudos
Reply
3,386 Views
vinothkumars
Senior Contributor IV

Hi,

Finally this one fixed by minimal u-boot binary (u-boot-spl.bin) instead of normal u-boot for sram.

Regards,
Vinothkumar Sekar
0 Kudos
Reply