VR5510 ABIST2 SVS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VR5510 ABIST2 SVS

1,986件の閲覧回数
zeyu_yan
Contributor III

Hi,

        for ASIL D ECU,if the SVS function of VR5510 is disable, should VR5510 enable the funciton of ABIST2?(since the voltages of PMIC do not change  )

0 件の賞賛
返信
2 返答(返信)

1,964件の閲覧回数
zeyu_yan
Contributor III

I understand that it will have no affect on ABIST2 if SVS is configured or not.

But if SVS is not configured, what is the meaning to enable ABIST2 while ABIST1 has already covered and checked the voltage error that ABIST2 do?

 

VR550-Flowchat.pngVR550-Flowchat.png

VR5510-ABIST.pngVR5510-ABIST.png

0 件の賞賛
返信

1,967件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

You can see the datasheet page20---8.14 Application flow charts,no affect on ABIST2.

0 件の賞賛
返信