VR5510 ABIST2 SVS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VR5510 ABIST2 SVS

2,034 Views
zeyu_yan
Contributor III

Hi,

        for ASIL D ECU,if the SVS function of VR5510 is disable, should VR5510 enable the funciton of ABIST2?(since the voltages of PMIC do not change  )

0 Kudos
Reply
2 Replies

2,012 Views
zeyu_yan
Contributor III

I understand that it will have no affect on ABIST2 if SVS is configured or not.

But if SVS is not configured, what is the meaning to enable ABIST2 while ABIST1 has already covered and checked the voltage error that ABIST2 do?

 

VR550-Flowchat.png

VR5510-ABIST.png

0 Kudos
Reply

2,015 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can see the datasheet page20---8.14 Application flow charts,no affect on ABIST2.

0 Kudos
Reply