UJA1169ATK Maximum SPI Clock Speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UJA1169ATK Maximum SPI Clock Speed

Jump to solution
2,993 Views
JarryZheng
Contributor I

The manual only sees that the minimum clock period is 250ns, but it does not tell me the maximum clock frequency.Can you tell me the maximum clock frequency supported by the SPI interface of the chip UJA1169ATK? Thank you!

BR

0 Kudos
Reply
1 Solution
2,983 Views
guoweisun
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
2 Replies
2,984 Views
guoweisun
NXP TechSupport
NXP TechSupport

Should be 4MHz.

0 Kudos
Reply
2,976 Views
JarryZheng
Contributor I

The clock frequency for SPI reads and writes must not exceed 4Mhz. Is that right?

0 Kudos
Reply