UJA1169ATK Maximum SPI Clock Speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UJA1169ATK Maximum SPI Clock Speed

Jump to solution
2,949 Views
JarryZheng
Contributor I

The manual only sees that the minimum clock period is 250ns, but it does not tell me the maximum clock frequency.Can you tell me the maximum clock frequency supported by the SPI interface of the chip UJA1169ATK? Thank you!

BR

0 Kudos
Reply
1 Solution
2,939 Views
guoweisun
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
2 Replies
2,940 Views
guoweisun
NXP TechSupport
NXP TechSupport

Should be 4MHz.

0 Kudos
Reply
2,932 Views
JarryZheng
Contributor I

The clock frequency for SPI reads and writes must not exceed 4Mhz. Is that right?

0 Kudos
Reply