SBC FS26 WAKEUP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SBC FS26 WAKEUP

Jump to solution
5,212 Views
mogilipuri_harish
Contributor II

hello team

 

we are using FS2633 and S32K144 uC in our design. 

 

1.how to wakeup SBC in when it is in Standby mode? in which pin we need to connect in micro the controller?

2. how to wake up SBC when it is low power mode?

0 Kudos
Reply
1 Solution
5,197 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Harish,

The FS26 can wake up from any of the Low Power modes via any of the following selectable wake-up mechanisms available in the device (availability is dependent on part number):

  • WAKE1 and WAKE2 pins
  • GPIO1 and GPIO2 pins
  • Long Duration Timer (LDT) expiration
  • SPI activity via edge detection of the CSB pin

The table below summarizes the operating modes and available wake-up sources.

Capture.JPG

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
5 Replies
5,198 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Harish,

The FS26 can wake up from any of the Low Power modes via any of the following selectable wake-up mechanisms available in the device (availability is dependent on part number):

  • WAKE1 and WAKE2 pins
  • GPIO1 and GPIO2 pins
  • Long Duration Timer (LDT) expiration
  • SPI activity via edge detection of the CSB pin

The table below summarizes the operating modes and available wake-up sources.

Capture.JPG

Best regards,

Tomas

0 Kudos
Reply
4,570 Views
Akhil1
Contributor I

Hello @TomasVaverka , Can you please send any example file reagrding SBC FS26 wakeup using LDT in s32k3 controller.

 

Thanks and Regards

Akhil

0 Kudos
Reply
5,138 Views
mogilipuri_harish
Contributor II

hi

 

can you please provide the wakeup pin current in SBC

 

0 Kudos
Reply
5,126 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Harish,

This is shown in Table 135 of the datasheet.

Capture.JPG

Best regards,

Tomas

0 Kudos
Reply
4,514 Views
Akhil1
Contributor I

Can you please provide an example for S32k312 wakeup using SBC FS26 using Long duration timer.

Regards

Akhil

0 Kudos
Reply