SBC FS26 WAKEUP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,156件の閲覧回数
mogilipuri_harish
Contributor II

hello team

 

we are using FS2633 and S32K144 uC in our design. 

 

1.how to wakeup SBC in when it is in Standby mode? in which pin we need to connect in micro the controller?

2. how to wake up SBC when it is low power mode?

0 件の賞賛
返信
1 解決策
5,141件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Harish,

The FS26 can wake up from any of the Low Power modes via any of the following selectable wake-up mechanisms available in the device (availability is dependent on part number):

  • WAKE1 and WAKE2 pins
  • GPIO1 and GPIO2 pins
  • Long Duration Timer (LDT) expiration
  • SPI activity via edge detection of the CSB pin

The table below summarizes the operating modes and available wake-up sources.

Capture.JPG

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
5,142件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Harish,

The FS26 can wake up from any of the Low Power modes via any of the following selectable wake-up mechanisms available in the device (availability is dependent on part number):

  • WAKE1 and WAKE2 pins
  • GPIO1 and GPIO2 pins
  • Long Duration Timer (LDT) expiration
  • SPI activity via edge detection of the CSB pin

The table below summarizes the operating modes and available wake-up sources.

Capture.JPG

Best regards,

Tomas

0 件の賞賛
返信
4,514件の閲覧回数
Akhil1
Contributor I

Hello @TomasVaverka , Can you please send any example file reagrding SBC FS26 wakeup using LDT in s32k3 controller.

 

Thanks and Regards

Akhil

0 件の賞賛
返信
5,082件の閲覧回数
mogilipuri_harish
Contributor II

hi

 

can you please provide the wakeup pin current in SBC

 

0 件の賞賛
返信
5,070件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Harish,

This is shown in Table 135 of the datasheet.

Capture.JPG

Best regards,

Tomas

0 件の賞賛
返信
4,458件の閲覧回数
Akhil1
Contributor I

Can you please provide an example for S32k312 wakeup using SBC FS26 using Long duration timer.

Regards

Akhil

0 件の賞賛
返信