Reduce transients in PF8100

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Reduce transients in PF8100

ソリューションへジャンプ
2,961件の閲覧回数
Ellu24
Contributor III

I am designing a hardware using LS1046 for space applications. I am using PF8100 and LTC7150 as in freeway board for the power supply.

1) Should I use and other devices (like TVS diode or zener diode) other than in freeway board to reduce the transients?

2) If I should use the above, where should I place the same?

 

Thanking you in advance.

0 件の賞賛
返信
1 解決策
2,946件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Here I give example for this part green circle:

guoweisun_0-1675826040631.png

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,954件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

If add the robustness performance on EMC test, you can add the TVS on input terminations of regulators.

According the EMC level to select the corresponding components.

 

 

0 件の賞賛
返信
2,953件の閲覧回数
Ellu24
Contributor III

Thank you very much for your prompt response. Can you please suggest any TVS diode for this application. As per design, I will get 5v of input voltage from 6 pin picoblade connector and then I should down convert that to 3.3.V(using LT8642) and 1V (LTC7150) and 3.3 V as the input of PMIC(PF8100). Where can I add the TVS? Should I filter the 5V power from ATX power supply?

 

Thanking you in advance.

0 件の賞賛
返信
2,947件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Here I give example for this part green circle:

guoweisun_0-1675826040631.png

 

 

0 件の賞賛
返信
2,940件の閲覧回数
Ellu24
Contributor III

Thank you very much for the details.

0 件の賞賛
返信