Reduce transients in PF8100

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Reduce transients in PF8100

跳至解决方案
2,982 次查看
Ellu24
Contributor III

I am designing a hardware using LS1046 for space applications. I am using PF8100 and LTC7150 as in freeway board for the power supply.

1) Should I use and other devices (like TVS diode or zener diode) other than in freeway board to reduce the transients?

2) If I should use the above, where should I place the same?

 

Thanking you in advance.

0 项奖励
回复
1 解答
2,967 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Here I give example for this part green circle:

guoweisun_0-1675826040631.png

 

 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,975 次查看
guoweisun
NXP TechSupport
NXP TechSupport

If add the robustness performance on EMC test, you can add the TVS on input terminations of regulators.

According the EMC level to select the corresponding components.

 

 

0 项奖励
回复
2,974 次查看
Ellu24
Contributor III

Thank you very much for your prompt response. Can you please suggest any TVS diode for this application. As per design, I will get 5v of input voltage from 6 pin picoblade connector and then I should down convert that to 3.3.V(using LT8642) and 1V (LTC7150) and 3.3 V as the input of PMIC(PF8100). Where can I add the TVS? Should I filter the 5V power from ATX power supply?

 

Thanking you in advance.

0 项奖励
回复
2,968 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Here I give example for this part green circle:

guoweisun_0-1675826040631.png

 

 

0 项奖励
回复
2,961 次查看
Ellu24
Contributor III

Thank you very much for the details.

0 项奖励
回复