Reduce transients in PF8100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reduce transients in PF8100

Jump to solution
2,932 Views
Ellu24
Contributor III

I am designing a hardware using LS1046 for space applications. I am using PF8100 and LTC7150 as in freeway board for the power supply.

1) Should I use and other devices (like TVS diode or zener diode) other than in freeway board to reduce the transients?

2) If I should use the above, where should I place the same?

 

Thanking you in advance.

0 Kudos
Reply
1 Solution
2,917 Views
guoweisun
NXP TechSupport
NXP TechSupport

Here I give example for this part green circle:

guoweisun_0-1675826040631.png

 

 

View solution in original post

0 Kudos
Reply
4 Replies
2,925 Views
guoweisun
NXP TechSupport
NXP TechSupport

If add the robustness performance on EMC test, you can add the TVS on input terminations of regulators.

According the EMC level to select the corresponding components.

 

 

0 Kudos
Reply
2,924 Views
Ellu24
Contributor III

Thank you very much for your prompt response. Can you please suggest any TVS diode for this application. As per design, I will get 5v of input voltage from 6 pin picoblade connector and then I should down convert that to 3.3.V(using LT8642) and 1V (LTC7150) and 3.3 V as the input of PMIC(PF8100). Where can I add the TVS? Should I filter the 5V power from ATX power supply?

 

Thanking you in advance.

0 Kudos
Reply
2,918 Views
guoweisun
NXP TechSupport
NXP TechSupport

Here I give example for this part green circle:

guoweisun_0-1675826040631.png

 

 

0 Kudos
Reply
2,911 Views
Ellu24
Contributor III

Thank you very much for the details.

0 Kudos
Reply