PMIC PF0100 Reference voltage issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PMIC PF0100 Reference voltage issue

4,311件の閲覧回数
jomsabu
Contributor I

The DDR reference voltage from PMIC giving 1.2v rather than .75v.How to solve this issue

0 件の賞賛
返信
5 返答(返信)

4,045件の閲覧回数
art
NXP Employee
NXP Employee

Do you mean the VREFDDR output of the PMIC? If so, please specify some more details. What voltage is applied to VINREFDDR? How VHALF is connected? Please provide the schematic of the PMIC connections.


Have a great day,
Artur

-

0 件の賞賛
返信

4,045件の閲覧回数
jomsabu
Contributor I

We have done power testing with PMIC MMPF0100F0AEP, all voltage levels are working fine except VREFDDR (half voltage of VINREFDDR-1.5V) .

Expecting voltage at VREFDDR is 0.75V but we found that as 1.2V.

Please go through the below image,

0 件の賞賛
返信

4,045件の閲覧回数
jomsabu
Contributor I

PMIC.JPG

0 件の賞賛
返信

4,045件の閲覧回数
art
NXP Employee
NXP Employee

The MMPF0100 PMIC doesn't have any internal mechanism to control the VREFDDR voltage, it can only be enabled/disabled internally. In normal conditions (all external circuits are connected correctly), the VREFDDR voltage is exactly the half of VINREFDDR. So, in your case, most likely there is some external side effect e.g. voltage leakage or short circuit. Please check. Also, check whether the VREFDDR voltage is enabled in the VREFDDCRTL register (bit 4 should be 1) of the PMIC.

Artur

0 件の賞賛
返信

4,045件の閲覧回数
art
NXP Employee
NXP Employee

Sorry, don't see any image here.

Artur

0 件の賞賛
返信