PF8100 VSNVS output Impossible Voltage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF8100 VSNVS output Impossible Voltage

16,990件の閲覧回数
chinachuli
Contributor II

when i modify "i.MX8QXP MEK schematic" to my own imx8qxp board, see attachment,i find VSNVS pin output at 5v, in datesheet VSNVS max output voltage is 3.3v. i do not know where is wrong, thanks for give me some suggesstion!

pastedImage_1.png

我在用官方IMX8QXP修改至自己的核心板,主要是简化了不必要的接口电路,原理图见附件,但我板子做回来测量发现VSNVS的输出有5V,而数据手册上最高电压为3.3V,找了很大时间未找出原因,所以求助论坛,非常感谢!

ラベル(2)
タグ(1)
0 件の賞賛
返信
8 返答(返信)

16,594件の閲覧回数
chinachuli
Contributor II

Simplify board to only have pmic part, schematic see attachment,VSNVS also output 5V, Where is wrong

0 件の賞賛
返信

16,595件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

Do you connect with light load on this VSNVS output then see the actual output?

0 件の賞賛
返信

16,594件の閲覧回数
chinachuli
Contributor II

when VSNVS load 1k ,the actual output still is 5V 

0 件の賞賛
返信

16,594件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Do you mind have a phone call with me?

Or give your phone number!

0 件の賞賛
返信

16,595件の閲覧回数
chinachuli
Contributor II

孙工:

我想用二层板做一块pf8100的测试板,原理图见附件。

在 2018-12-04 13:17:36,"褚立" <chinachuli@163.com> 写道:

HI:

我的电话:18158182825 褚立 非常感谢!

0 件の賞賛
返信

16,595件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

可以这样做,或者你能预留一个Li-ion battery的位置方便调试,拉出来IIC的信号出来。

0 件の賞賛
返信

16,594件の閲覧回数
chinachuli
Contributor II

HI:

我的电话:18158182825 褚立 非常感谢!

0 件の賞賛
返信

16,594件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

This should not PMIC's issue,you can disconnect VSNVS with your system only test VSNVS output to check PMIC good or not.

0 件の賞賛
返信