TEA19161Control of turn ratio (TEA19161匝比不同的设计方法)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEA19161Control of turn ratio (TEA19161匝比不同的设计方法)

3,634 Views
184156532
Contributor I

TEA19161Control of turn ratio

TEA19161

用谐振式SMPS设计工具设计

Design of Resonant SMPS Design Tool

例:input:390VDC OUPUT:24V7.5A 变压器匝比为:34:4:4 748UH Lr:115 Cr:433

Example: input: 390VDC OUPUT: 24V7.5A transformer turn-to-turn ratio: 34:4:4 748UH Lr:115Cr:433

实际用半桥计算:(390/34)*4T/0.5=22.9V

Actual half-bridge calculation:34:4:4  (390/34)*4T/0.5=22.9V?

而32:4:4更符合匝比:(390/32)*4T/0.5=24.37V

32:4:4 is more in line with turn ratio: (390/32)*4T/0.5 = 24.37V?

Which is correct?

TEA19161匝比不同的设计方法
用谐振式SMPS设计工具设计时的匝比与常规计算差异产生的原因与哪个更符合实用?
例:input:390VDC  OUPUT:24V7.5A   变压器匝比为:34:4:4 748UH Lr:115 Cr:433
实际用半桥计算:(390/34)*4T/0.5=22.9V
而32:4:4更符合匝比:(390/32)*4T/0.5=24.37V
匝比控制问题
哪个正确?

Labels (1)
0 Kudos
Reply
1 Reply

2,724 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

建议你还是用design tool设计的结果!

0 Kudos
Reply