PF5020 PMIC – OTP Protection and Communication Sequence Clarification

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PF5020 PMIC – OTP Protection and Communication Sequence Clarification

跳至解决方案
393 次查看
Shivani_Elavena
Contributor II

Hi,

We have integrated the PF5020 PMIC with an NXP controller(IMXRT1176), and we have a couple of questions:

  1. Is there a specific register bit or method to disable or lock out OTP (One-Time Programming) to prevent accidental writes during development? If it is, then provide a detail document or description.

  2. The datasheet doesn’t show a detailed I2C communication read/write sequence. Is there any reference document or application note that outlines the proper sequence for safe register access?

Thanks in advance for your help.

Best regards,
Shivani 

 

0 项奖励
回复
1 解答
375 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi Shivani 

  1. Is there a specific register bit or method to disable or lock out OTP (One-Time Programming) to prevent accidental writes during development? If it is, then provide a detail document or description.[gw]No there is no.

  2. The datasheet doesn’t show a detailed I2C communication read/write sequence. Is there any reference document or application note that outlines the proper sequence for safe register access?

        [gw]Please see attached.

在原帖中查看解决方案

0 项奖励
回复
1 回复
376 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi Shivani 

  1. Is there a specific register bit or method to disable or lock out OTP (One-Time Programming) to prevent accidental writes during development? If it is, then provide a detail document or description.[gw]No there is no.

  2. The datasheet doesn’t show a detailed I2C communication read/write sequence. Is there any reference document or application note that outlines the proper sequence for safe register access?

        [gw]Please see attached.

0 项奖励
回复