PF3000 PWRON Pull-down resistor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF3000 PWRON Pull-down resistor

Jump to solution
2,302 Views
HOTA
Contributor III

Hi,

Does the PF3000 PWRON (48 Pin) have an implemented internal pull-down or pull-up resistor? Additionally, when applying a high signal externally, what would be the leakage current in Amps?

 

Thanks,

HOTA

0 Kudos
Reply
1 Solution
2,288 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Hota,

There is no internal pull-up or pull-down resistor on the PWRON pin and the leakage current is negligible, definitely not in Amps.

BR, Tomas

View solution in original post

2 Replies
2,289 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Hota,

There is no internal pull-up or pull-down resistor on the PWRON pin and the leakage current is negligible, definitely not in Amps.

BR, Tomas

2,285 Views
HOTA
Contributor III

Hi Tomas,

 

Thank you for your clear answer. My question has been resolved.

 

Thanks,

Ohta

0 Kudos
Reply