PF3000 PWRON Pull-down resistor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PF3000 PWRON Pull-down resistor

跳至解决方案
2,301 次查看
HOTA
Contributor III

Hi,

Does the PF3000 PWRON (48 Pin) have an implemented internal pull-down or pull-up resistor? Additionally, when applying a high signal externally, what would be the leakage current in Amps?

 

Thanks,

HOTA

0 项奖励
回复
1 解答
2,287 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Hota,

There is no internal pull-up or pull-down resistor on the PWRON pin and the leakage current is negligible, definitely not in Amps.

BR, Tomas

在原帖中查看解决方案

2 回复数
2,288 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Hota,

There is no internal pull-up or pull-down resistor on the PWRON pin and the leakage current is negligible, definitely not in Amps.

BR, Tomas

2,284 次查看
HOTA
Contributor III

Hi Tomas,

 

Thank you for your clear answer. My question has been resolved.

 

Thanks,

Ohta

0 项奖励
回复