PF3000 PWRON Pull-down resistor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF3000 PWRON Pull-down resistor

ソリューションへジャンプ
2,300件の閲覧回数
HOTA
Contributor III

Hi,

Does the PF3000 PWRON (48 Pin) have an implemented internal pull-down or pull-up resistor? Additionally, when applying a high signal externally, what would be the leakage current in Amps?

 

Thanks,

HOTA

0 件の賞賛
返信
1 解決策
2,286件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Hota,

There is no internal pull-up or pull-down resistor on the PWRON pin and the leakage current is negligible, definitely not in Amps.

BR, Tomas

元の投稿で解決策を見る

2 返答(返信)
2,287件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Hota,

There is no internal pull-up or pull-down resistor on the PWRON pin and the leakage current is negligible, definitely not in Amps.

BR, Tomas

2,283件の閲覧回数
HOTA
Contributor III

Hi Tomas,

 

Thank you for your clear answer. My question has been resolved.

 

Thanks,

Ohta

0 件の賞賛
返信