PF0200 capacitive load

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF0200 capacitive load

ソリューションへジャンプ
4,153件の閲覧回数
victorafanasiev
Contributor II

In my board, based on the MCIMX6X2AVN08AB microprocessor, I use the PMIC MMPF0200F6AEP as a power supply. The output SW2 of the MMPF0200F6AEP chip is used not only to power the microprocessor MCIMX6X2AVN08AB itself but also to power the FPGA Spartan6 type. The FPGA Spartan6 requires using of large decoupling capacitors. Tell me please, what is the maximum permissible value of the capacitive load on the SW2 output (and others) of the MMPF0200F6AEP chip?

0 件の賞賛
返信
1 解決策
3,950件の閲覧回数
victorafanasiev
Contributor II

Hi, Jose. Thanks for your reply.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,950件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

MAX capacitance for the SW2 output is not characterized, but I recommend you to use the 3 x 22 uF capacitors as recommended in the datasheet on Table 62.

 

We have seen that customer that add extra capacitance on the buck regulators, typically increase the desired voltage level on the line.

 

I’m worried about the current capabilities of the SW2 to supply both systems (IMX6 and FPGA), SW2 can give up to 2.5A (with a supply between 1.2V and 3.3V).


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,951件の閲覧回数
victorafanasiev
Contributor II

Hi, Jose. Thanks for your reply.

0 件の賞賛
返信