PF0200 capacitive load

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF0200 capacitive load

Jump to solution
4,128 Views
victorafanasiev
Contributor II

In my board, based on the MCIMX6X2AVN08AB microprocessor, I use the PMIC MMPF0200F6AEP as a power supply. The output SW2 of the MMPF0200F6AEP chip is used not only to power the microprocessor MCIMX6X2AVN08AB itself but also to power the FPGA Spartan6 type. The FPGA Spartan6 requires using of large decoupling capacitors. Tell me please, what is the maximum permissible value of the capacitive load on the SW2 output (and others) of the MMPF0200F6AEP chip?

0 Kudos
Reply
1 Solution
3,925 Views
victorafanasiev
Contributor II

Hi, Jose. Thanks for your reply.

View solution in original post

0 Kudos
Reply
2 Replies
3,925 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

MAX capacitance for the SW2 output is not characterized, but I recommend you to use the 3 x 22 uF capacitors as recommended in the datasheet on Table 62.

 

We have seen that customer that add extra capacitance on the buck regulators, typically increase the desired voltage level on the line.

 

I’m worried about the current capabilities of the SW2 to supply both systems (IMX6 and FPGA), SW2 can give up to 2.5A (with a supply between 1.2V and 3.3V).


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,926 Views
victorafanasiev
Contributor II

Hi, Jose. Thanks for your reply.

0 Kudos
Reply