PCA9420 (How to change SW2 default 1.8V output to 3.3V output)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA9420 (How to change SW2 default 1.8V output to 3.3V output)

ソリューションへジャンプ
976件の閲覧回数
Selamu
Contributor I

Hi community,

We use a PCA9420 PMIC on our design and would like to change BUCK2 (SW2, system buck regulator) default 1.8V output to 3.3V. I checked the datasheet and it shows that, on page 15, the SW2 output voltage can be programmed via I2C register from 1.5V to 2.1V, or from 2.7V to 3.3V in both at 25mV/step, but the maximum voltage which is available to select on all mode settings is 2.1V.

anybody has an idea on how it will be changed to 3.3V?

Regards

0 件の賞賛
返信
1 解決策
966件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Selamu,

In order to set SW2 output voltage in the range of 2.7V to 3.3V, the SW2_OUT_1_OFFSET bit needs to be set to 1:

Table 54.JPG

Then SW2 Output Voltage = SW2_OUT_1_LSB[4:0] + 1.2V, so if you set SW2_OUT_1_LSB[4:0] = 0b11001-0b11111 = 2.1V, then SW2 = 2.1V + 1.2V = 3.3V

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
967件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Selamu,

In order to set SW2 output voltage in the range of 2.7V to 3.3V, the SW2_OUT_1_OFFSET bit needs to be set to 1:

Table 54.JPG

Then SW2 Output Voltage = SW2_OUT_1_LSB[4:0] + 1.2V, so if you set SW2_OUT_1_LSB[4:0] = 0b11001-0b11111 = 2.1V, then SW2 = 2.1V + 1.2V = 3.3V

Best regards,

Tomas

0 件の賞賛
返信