PCA9420 (How to change SW2 default 1.8V output to 3.3V output)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PCA9420 (How to change SW2 default 1.8V output to 3.3V output)

跳至解决方案
961 次查看
Selamu
Contributor I

Hi community,

We use a PCA9420 PMIC on our design and would like to change BUCK2 (SW2, system buck regulator) default 1.8V output to 3.3V. I checked the datasheet and it shows that, on page 15, the SW2 output voltage can be programmed via I2C register from 1.5V to 2.1V, or from 2.7V to 3.3V in both at 25mV/step, but the maximum voltage which is available to select on all mode settings is 2.1V.

anybody has an idea on how it will be changed to 3.3V?

Regards

0 项奖励
回复
1 解答
951 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Selamu,

In order to set SW2 output voltage in the range of 2.7V to 3.3V, the SW2_OUT_1_OFFSET bit needs to be set to 1:

Table 54.JPG

Then SW2 Output Voltage = SW2_OUT_1_LSB[4:0] + 1.2V, so if you set SW2_OUT_1_LSB[4:0] = 0b11001-0b11111 = 2.1V, then SW2 = 2.1V + 1.2V = 3.3V

Best regards,

Tomas

在原帖中查看解决方案

0 项奖励
回复
1 回复
952 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Selamu,

In order to set SW2 output voltage in the range of 2.7V to 3.3V, the SW2_OUT_1_OFFSET bit needs to be set to 1:

Table 54.JPG

Then SW2 Output Voltage = SW2_OUT_1_LSB[4:0] + 1.2V, so if you set SW2_OUT_1_LSB[4:0] = 0b11001-0b11111 = 2.1V, then SW2 = 2.1V + 1.2V = 3.3V

Best regards,

Tomas

0 项奖励
回复